Technical FAQs

Ask a Question

What is the max cable distance you can run on the ATV32 drives before having to add a output load reactor?

Issue:
What is the max cable distance you can run on the ATV32 drives before having to add a output load reactor?

Product Line:
Altivar ATV32

Environment:
All 

Cause:
Needs to know the max cable distance you can run the drive before adding a load reactor. 

Resolution:
See the ATV32 motor choke table below.






 
Was this helpful?
What can we do to improve the information ?