Technical FAQs

Ask a Question

What is the maximum operating current of the MPPT 80?

Issue
Maximum Operating Current for the MPPT 80 600

Product Line
MPPT 80

Environment
Installation using the MPPT 80

Cause
The operating current is not listed on the data sheet for the MPPT 80 600.

Resolution
Operating current for the MPPT 80 600 is 23A.  This information can be found under the "Electrical Specifications" section of the MPPT 80 600 Owner's Guide.  
Was this helpful?
What can we do to improve the information ?