Technical FAQs

Ask a Question

Can I change the font size in SoMachine Basic?

Issue:
Can I change the font size in SoMachine Basic?

Product Line:
SoMachine Basic

Resolution:
Unfortunately, the SoMachine Basic does not have a zoom in/out to the programming window.
You can expand the programming columns but the font size will still be the same.
To expand the columns, you should go to the toolbar and click the Setup icon (wrench and hammer icon - See attached)
Was this helpful?
What can we do to improve the information ?