Technical FAQs

Ask a Question

How do I remove the Front Cover to connect the Modbus Serial cable to the Modbus serial port on the Altivar 600 Process Drive?

 Issue:
How do I remove the Front Cover to connect the Modbus Serial cable to the Modbus serial port on the Altivar 600 Process Drive?

Product Line:
Altivar 600 Process Drive

Environment:
All serial numbers for Altivar 600 Process Drive

Cause:
N/A

Resolution:



Procedure to Remove the Front Cover of the Drive

1 Unscrew the four screws attaching the front cover
2 Slide down the front cover
3 Remove the front cover
4 Plug the Modbus serial cable in the Modbus serial port





 
Was this helpful?
What can we do to improve the information ?