Technical FAQs

Ask a Question

What are the pin-outs for the Embedded Modbus RJ45 Connector on the Altivar Process Drive?

Issue:
What are the pin-outs for the Embedded Modbus RJ45 Connector on the Altivar Process Drive?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
The following figure shows the pin layout for RJ45 connector:




 
Was this helpful?
What can we do to improve the information ?