Technical FAQs

Ask a Question

Where do I connect the Auto Start contacts on an 8839EFD with HOA switch?

Issue:
Where do I connect the Auto Start contacts on an 8839EFD with HOA switch?
 
Product Line:
8839 EFD
 
Environment:
Power Circuit Y (With Bypass): Hand-Off-Auto and Speed Potentiometer
 
Cause:
Remote start
 
Resolution:


 
Was this helpful?
What can we do to improve the information ?