Technical FAQs

Ask a Question

Does the 2510MCG1 manual strater require 1 or 2 thermal units?

Issue;
How many thermal units are required for 2510MCG1

Product Line;
Manual Starter

Environment;
2510 Manual Motor Starter 

Cause;
Thermal units

Resolution;
It is one thermal unit
 
Was this helpful?
What can we do to improve the information ?