Technical FAQs

Ask a Question

What is the replacement part number for Lexium 05 drive bearing part number LXM05AD42M3X?

Issue:
What is the replacement part number for Lexium 05 drive bearing part number LXM05AD42M3X?

Product Line:
LXM05, LXM32

Resolution:
The corresponding part number to replace a LXM05AD14N4 will be a LXM32MD30N4 in terms of current rating.
If CANOpen was used to control the LXM05, a CANOpen card has to be added: VW3A3608
If motor's date of manufacture (DOM) is older than 15.07.2009, a firmware upgrade of the motor is required to work with the new LXM32 drive.

 
Was this helpful?
What can we do to improve the information ?