Technical FAQs

Ask a Question

How is the RAM DBS P9 CT connector repaired or replaced?

Issue:
How is the RAM DBS P9 CT connector repaired replaced?
 
Product Line:
DBS
 
Environment:
All models
 
Cause:
P9 connector damage.
Discolored connector from overheating.  See attached file.
This will cause nuisance phase loss trips and incorrect amp readings.
 
Resolution:
The P9 connector was used on the first generation DBS board set.  That type connector is not used on the DBS II board set and is not available.  Order a board set conversion kit, RAM-400339-KIT.  It includes the current version board set and a new TB2 connector for the CT wires. See attached file.

Was this helpful?
What can we do to improve the information ?