Technical FAQs

Ask a Question

Is there a Conduit Kit available for ATV71HC31N4 drive?

Issue:
Is there a Conduit Kit available for ATV71HC31N4 drive?

Product Line:
Altivar 71, ATV71

Environment:
ATV71HC31N4

Cause:
NA

Resolution:
There is not a conduit kit available for the ATV71HC31N4.
For ATV71  380V, the accessory is only  available up to ATV71HC28N4 .
But for ATV61  380V, the accessory is  available up to ATV61HC31N4.
And there is the VW3A9115 conformity kit available in Europe for the ATV71HC31N4.
Was this helpful?
What can we do to improve the information ?