Technical FAQs

Ask a Question

Monitoring PWR on EtherCAT

Issue:
Can PWR Status be monitored over EtherCAT?

Product Line:
Altivar drives

Environment:
All

Cause:
N/A

Resolution:
There is no address for Logic input of Power removal to monitor. But you can check this HMIS register ( CANopen adress Index: 16#2002, SubIndex:29 ).

If the value of this register is equal to 12, means that the  Power removal is activated.

FYI. If at first the drive is in nLp ( no power, only external 24V). The HMIS=11 "nLP", but then if the power removal is activated, HMIS=12 "PrA". PrA has the priority compared to "nLP".
Then if drive trips in fault. HMIS will be equal to 23 "FLt". FLt has the priority compared to "PrA".
Was this helpful?
What can we do to improve the information ?