Technical FAQs

Ask a Question

Can PWR Status be monitored over EtherCAT?

Issue:
Can PWR Status be monitored over EtherCAT?

Product Line:
Altivar drives, ATV71, ATV61

Environment:
All

Cause:
N/A

Resolution:
There is no address for Power removal Logic Input to monitor.
However, you can check the HMIS register ( CANopen address Index: 16#2002, SubIndex:29 ).
If the value of this register is equal to 12, means that the  Power removal is activated.

Note: If at first the drive is in nLp ( no line power, only external 24V). The HMIS=11 "nLP", but then if the power removal is activated, HMIS=12 "PrA". PrA has the priority over "nLP".
Then if drive trips in fault. HMIS will be equal to 23 "FLt". FLt has priority over "PrA".
Was this helpful?
What can we do to improve the information ?