Technical FAQs

Ask a Question

Looking to buy Berger Lahr STA5-B0-36/8-3N23L

Issue:
Looking to buy Berger Lahr STA5-B0-36/8-3N23L

Product Line:
Berger Lahr

Resolution:
The STA5-B0.36/83N23-L is a customized actuator. 
These products are specialized and their sale is limited to the OEM machine builders. 
Unfortunately, it's not available for purchase to the end-user directly from Schneider Electric. 
The customer must contact the Original Equipment Manufacturer of the machine to get a spare.
Was this helpful?
What can we do to improve the information ?