Technical FAQs

Ask a Question

What is the difference in a PAF and an SPAF circuit breaker?

Product Line:
Circuit Breakers

PAF and SPAF Circuit Breakers
PHF and SPHF Circuit Breakers
PCF and SPCF Circuit Breakers

When they were available, the PAF and SPAF were the same physical size, but the PAF breakers were UL listed and the SPAF breakers were IEC listed. In a similar manner, the PHF and PCF were UL listed, but the SPHF and SPCF were IEC listed.

All of these breakers are now obsolete.
Was this helpful?
What can we do to improve the information ?