Technical FAQs

Ask a Question

What is the distance between the plug in openings for AP and CP 800 - 5000A busway?

Issue:
What is the distance between the plug in openings for AP and CP 800 - 5000A busway?

Product Line:
Busway

Environment:
I-line II Plug in style AP and CP Busway

Cause:
Product features and dimensions

Resolution:
On a 10 foot length of plug in style 800 - 5000A busway, the distance is 24" center line to center line of the plug in openings. There is a 12" distance from either end to the first plug opening.
Was this helpful?
What can we do to improve the information ?