Technical FAQs

Ask a Question

What do fault codes 0010, 0011, 0012 & 0013 mean?

Inverter keeps faulting on frequency and voltage faults.

Product Line:
PV and GT Series

Grid event: The grid frequency or grid voltage are out of range.

Grid event

When there is a frequency or voltage issue (High or Low) that is outside of the inverters allowable range, the inverter will shutdown. This is a grid related event. The inverter will stay down until the grid issue has been resolved. The inverter will start up automatically once the grid is back to normal.
If it does not, please call 866-519-1470 (option 3 & 3) to open a new case.
Was this helpful?
What can we do to improve the information ?