Technical FAQs

Ask a Question

What is the part number for the communication module adapter used for the Altivar 320 drives?

Issue:
What is the part number for the communication module adapter used for the Altivar 320?

Product Line:
ATV320

Environment:
All ATV320 compact versions

Cause:
Communication module does not fit.

Resolution:
VW3A3600
The communication module adapter is only required for the Altivar 320 compact version.
Was this helpful?
What can we do to improve the information ?