Technical FAQs

Ask a Question

Can SoMove connect to multiple drives via Bluetooth?

Issue:
Bluetooth connections

Product Line:
ATV12, ATV32, ATV312, ATV212, ATV61, ATV71, ATV630, ATV930

Environment:
All bluetooth capable drives using the internal bluetooth enable (ATV32) or those with the bluetooth dongle (pn: TCSWAAC13FB).

Cause:
None

Resolution:
SoMove connection via Bluetooth is point-to-point only.  So, you can be connected to one drive at a time.

Setting Multipoint/Monopoint is changing the scanned address only but does not organize any multi session.
Respectively, following drive's addresses are scanned:
Multipoint - 248
Monopoint - the address which is entered 0...247.

Each drive discovered on Bluetooth, reserves 2 COM ports:
 
Was this helpful?
What can we do to improve the information ?