Technical FAQs

Ask a Question

Can I replace the IO modules that come with the M258 controller from the CPU module?

Issue:
Can I replace the IO modules that come with the M258 controller from the CPU module?

Product Line:
TM258

Resolution:
No, these embedded IOs cannot be removed or replaced as this will fault out the controller.
You can only replace the terminal part of the IO modules, where the wires are plugged in.
Was this helpful?
What can we do to improve the information ?