Technical FAQs

Ask a Question

Can I disable a TM3 module in SoMachine?

Issue:
Set the TM3 module as optional in SoMachine

Product Line:
Modicon TM3

Resolution:
It's possible to set a TM3 module as optional in SoMachine. This will allow you to run your program without faulting the TM3 bus even if the TM3 module is not physically present on the rack. 
See attached for how to do that in SoMachine. 
Was this helpful?
What can we do to improve the information ?