Technical FAQs

Ask a Question

What is the warranty on the SDSA1175, SDSA3650, and XR Series Surge Protective Devices (SPDs)?

Product Line: 
Surge Protective Devices (SPDs)

Enviorment:
SDSA1175, SDSA3650, and XR Series Warranty

Resolution:
If the device has been properly installed in compliance with all applicable electrical code requirements, Square D warrants the SPD to be free from defects in materials and workmanship for a period of two (2) years from date of invoice from Square D or its authorized sales channel.
Was this helpful?
What can we do to improve the information ?