Technical FAQs

Ask a Question

Are the Altivar 630 and Altivar 930 Process Drive available?

Issue:
Are the Altivar 630 and Altivar 930 Process Drive available?

Product Line:
Altivar Process Drive (ATV630, ATV930)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
Altivar 630/930 (IP21)  
-  
Available as of third quarter of 2016 for 208/230V and 460V
-  Not available in 575/600V yet.

Altivar 630F/930F Floor Standing (IP55) 
- Not Available yet
Was this helpful?
What can we do to improve the information ?