Technical FAQs

Ask a Question

What is the part number for the 8536SA, SB, SC Overload-to-contactor fastening screw?

Issue:
Missing screw that holds the overload to the contactor. For a NEMA size 00, 0, or 1 device. 

Product Line: 
NEMA Contactors and Starters

Environment:
North American Products

Cause:
Lost / Missing screw 

Resolution:
The part number is
 3001807050. This consists of 1 piece wire clamp + 1 piece screw. 
Was this helpful?
What can we do to improve the information ?