Technical FAQs

Ask a Question

Is there a 125A 480V 3ph 65K Powerpact Type LJ circuit breaker?

Answer
Issue:
125A L-Frame breaker

Product Line:
Powerpact L - Frame Breaker

Environment:
Circuit breaker

Cause:
Catalog Selection

Resolution:
No, but LJL36250U31X is a standard trip 250A and can be dialed down to 70A. 

Keywords:
LJ, Powerpact L, L Frame, LJL, LJL36250U31X, LD, LG, LR, LL
 
Was this helpful?
What can we do to improve the information ?