Technical FAQs

Ask a Question

HTTP 500 Error: Can the Combox support Port Forwarding?

Issue:
User needs to port forward the Combox from local router to external router/network. Log in screen shows HTTP 500 Error. 

Product Line:
Conext Combox

Environment:
Conext Combox
Networking

Cause:
Mis-configuration of port on Dynamic IP Router

Resolution:
Schneider Electric does not Support or Recommend Port Forwarding on Conext Combox as it is insecure. 
In the case where users like to perform port forwarding, please use Dynamic IP Router and TCP Port 80. 
Combox does support TCP Port 80 for data transmission. 
 
Was this helpful?
What can we do to improve the information ?