Technical FAQs

Ask a Question

How come we are not getting any continuity on our 2510 manual starter?

 

Product Line:
2510 type F fractional horsepower manual starters

Environment:
Products sold and used in the United States

Cause:
Selection options for lower full load current thermal units for the 2510 type F manual motor starers.

Resolution:
They need to install the thermal units properly to obtain continuity, see below for the installation photos
Was this helpful?
What can we do to improve the information ?