Technical FAQs

Ask a Question

Wiring adapter LAD4BB

Issue:
With what units is the LAD4BB compatible?

Product Line:
IEC Contactors and Relays - GIC Product

Environment:
US Product

Cause:
Product compatibility

Resolution:
The LAD4BB can be used with any AC coil contactor LC1D09-LC1D38 or any AC coil CAD relay.  Please note that these wiring adapters are not compatible with DC coil units or units which are also using a coil suppressor.
Was this helpful?
What can we do to improve the information ?