Technical FAQs

Ask a Question

How to use the Micrologic P and H trip unit screen to seen the how much current is flowing through the breaker

Issue:
Is there a way to see the amount of load current in a Masterpact or Powerpact breaker?
Where is the amount of load current actually shown?

Product Line:
Circuit Breakers

Environment:
Applies to breakers with Micrologic P or H trip units

Resolution:
The amount of load current in each phase can be easily seen on the P or H trip unit screen. It will change as the load current changes.
Use the pictures below as a reference.

                                   Step 1



                                   Step 2



                                   Step 3



                                   Step 4



                                   Step 5
Was this helpful?
What can we do to improve the information ?