Technical FAQs

Ask a Question

Video: How to install LV426922 rear insulation screen onto Powerpact B-frame circuit breaker

Issue:
How do you install the rear insulation screen (LV426922) onto a B-frame breaker?
 
Product Line:
Molded Case Circuit Breakers
 
Environment:
B-Frame Circuit Breakers
 
Cause:
How do you install the rear insulation screen (LV426922) onto a B-frame breaker?
 
Resolution:
 
Insert the two notches on the screen into the two grooves on the back of the circuit breaker. For more information, see the video below or the attached instruction bulletin.

[video placeholder]
Was this helpful?
What can we do to improve the information ?