Technical FAQs

Ask a Question

Getting compile error 'Overlapping memory' in SoMachine

Issue:
Getting compile error 'Overlapping memory' in SoMachine

Product Line:
SoMachine

Resolution:
You must be using direct addressing while declaring variables for this to happen.
This compile error shows you which variables are overlapping.
If the concerned variables do not overlap (false alarm) but only belong to the same memory block (example MX10.0 and MX10.1), you can disable this verification in SoMachine by going to
Project Settings > Static Analysis Light > Uncheck 'Overlapping memory areas'
Was this helpful?
What can we do to improve the information ?