Technical FAQs

Ask a Question

What is F65 on my Conext SW?

Issue
F65 is not listed in Conext SW manual, but shows as AC Overload in the SCP.

Product Line
Conext SW 2524, 4024, 4048

Environment
Any Conext SW installation

Resolution
F65 is another method of checking for AC Overload.  Fault 64 measures the current on the secondary of the transformer.  Fault 65 measures the current on the DC input.  If you have fault 65, it's most likely caused by a failed power bridge.  It's shutting down the unit before any further damage can happen. 

Cause
F65 is a new fault that was added in the v3.06 firmware.  Included documentation and documentation available on sesolar.com have not yet been updated to include this fault.
Was this helpful?
What can we do to improve the information ?