Technical FAQs

Ask a Question

Can you monitor current on a 277V line with RM17JC00MW

Issue:
Can the RM17JC00MW be used to monitor current on a 277V line?

Product Line:
Current Measurment Relays - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
Yes, this product can be used to monitor current on a 277V line.  The only restriction is 20A or less.
Was this helpful?
What can we do to improve the information ?