Technical FAQs

Ask a Question

What are the differences between an ATV21 and an ATV212 drive?

Issue:
What are the differences between an ATV21 and an ATV212 drive?

Product Line:
Altivar 21
Altivar 212

Environment:
All

Cause:
Crossing from legacy to ATV212

Resolution:
 

Was this helpful?
What can we do to improve the information ?