Technical FAQs

Ask a Question

Are both the long and short wire binding screws included in lug kits AL175JD and AL250JD?

Issue:
Are both the long and short WBS included in the AL175JD and AL250JD lug kits?
What comes with the AL175JD?
What comes with the AL250JD?

Product Line:
Circuit Breakers

Environment:
Applies to Powerpact J

Resolution:
AL175JD
  • The AL175JD lug kit includes 3 lugs, each with the long wire binding screw (short WBS not included).
AL250JD
  • The AL250JD lug kit includes 3 lugs, each with the short wire binding screw (long WBS not included).
Was this helpful?
What can we do to improve the information ?