Technical FAQs

Ask a Question

How many switches can be on each pole of a lighting contactor?

There is no limit to the number of switches you can have downstream of the contactor. The limiting factors are the total current draw of the loads on the circuit and the current rating of the breaker feeding the circuit per NEC.

CTA-ID : 136
Was this helpful?
What can we do to improve the information ?