Technical FAQs

Ask a Question

What is the operating temperature range for NEMA rated lighting contactors?

The operating range for Class 8903 Type S and Type L(X) is 0 - 40 degrees Centigrade.


CTA-ID : 199
Was this helpful?
What can we do to improve the information ?