Technical FAQs

Ask a Question

Does Square D offer a 3 pole version of the 2510 type F starter?

Issue: Does Square D offer a 3 pole version of the 2510 type F starter?

Product Line: 2510 type F manual sarters

Environment: Products sold and used in the United States

Cause: would like a 3 pole 2510 type F fractional horse power (FHP) manual starter

Resolution: No, these starters are rated for single phase and DC applications only, consider Class 2510 Type M for three phase applications.


CTA-ID : 894
Was this helpful?
What can we do to improve the information ?