Technical FAQs

Ask a Question

What is the filler plate for branch breakers for the NF panel?

Issue:
What is the filler plate for branch breakers for the NF panelboard?

Product Line:
NF panelboards sold and supported in the USA.

Environment:
Maintenance/replacement/repair

Cause:
Filler plate requirement

Resolution:
EFP is the one pole filler plate.  For a two pole opening, use two filler plates; for three pole, use three filler plates.


Revised 3/10/04






CTA-ID : 624
Was this helpful?
What can we do to improve the information ?