Technical FAQs

Ask a Question

Are the Class 8903 Lighting Contactors rated for 600 volts?

Yes, up to and including 600 VAC, 50 or 60 hertz.


CTA-ID : 719
Was this helpful?
What can we do to improve the information ?