Technical FAQs

Ask a Question

What is the AIR rating for the Mag-Gard circuit breakers?

The Mag-Gard breakers have no stand alone interrupting rating. The Mag-Gard is a UL-recogonized component only. The interrupting rating is a combination rating with the motor starter and the Mag-Gard tested as a unit.


CTA-ID : 450
Was this helpful?
What can we do to improve the information ?