Technical FAQs

Ask a Question

Does Square D still offer TRILLIANT load center branch circuit breakers?

Issue:
Are the Trilliant load centers and breakers still available?

Product Line:
Trilliant Load Centers

Environment:
Branch Breakers

Cause:
Replacement

Resolution:
Most of the Trilliant branch circuit breakers are obsolete and no longer available, with no replacement.  Any Trilliant branch breakers that are still available would be loaded in the system.  An example of a trilliant branch breaker catalog number would be SDT120 (single pole, 20amp).  The only option is to replace the complete load center.
Was this helpful?
What can we do to improve the information ?