Technical FAQs

Ask a Question

Do we have an MEF36250LIG?

Product Line:
Legacy breaker ME/MX

The MEL / ME / MXL / MX breakers are obsolete. They are replaced by the Powerpact P frame breakers. The I-Line versions PJA will be direct replacements. However, the unit mount breakers are similar in size but are a little different so mounting, bus bar and sheetmetal may need to be changed. Services  can do a retrofit to substitute these breakers.

CTA-ID : 2000
Was this helpful?
What can we do to improve the information ?