Technical FAQs

Ask a Question

What is a handle padlock attachment for a FDA34070?

Issue:
Need to lock off handle on FDA,FGA,FJA I-line breakers

Product line:
I-line breakers

Environment:
I-Line panelboards and switchboards

Cause:
Need to lock the handle in OFF position for maintenance or safety.

Resolution:
Use the HPAFD lock off device.
HPAFD is a removable padlock attachment to lock the breaker "On" or "OFF". No fixed padlock attachment is available for these breakers.
At this time only the FJA 1P breakers are available. The FD, FG and 2P and 3P FJ breakers are obsolete.
Can be used with a padlock (provided by customer) or the screw that is included in kit.

 
Was this helpful?
What can we do to improve the information ?