Technical FAQs

Ask a Question

Powerpact phasing? FDA14020A?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Powerpact I-Line uses numbers rather than letters for phase option numbering.

1 pole A phase = 1, B=3, C=5 example FDA140201.
2 pole AB=1, AC=2, BA=3, BC=4, CA=5, CB=6 .
3 pole standard ABC no letter, CBA=6 .

See appropriate I-Line Digest page for particular circuit breaker information.
 
Was this helpful?
What can we do to improve the information ?