Technical FAQs

Ask a Question

What is the part number for a replacement 480-volt control coil for Class 8502 or Class 8536 Type SD contactor/starter?

31063-409-57 for 2 or 3 pole devices, 31063-400-57 for 4 or 5 pole devices; both coils are 480-volt 60-hertz or 440-volt 50 -hertz.


CTA-ID : 1465
Was this helpful?
What can we do to improve the information ?