Technical FAQs

Ask a Question

Q1 Circuit Breaker Replacement in obsolete NQO Panelboard

Issue:
What is the replacement for a Q1 circuit breaker in an obsolete NQO panelboard?

Product Line:
Obsolete NQO panelboards and Q1 circuit breakers

Environment:
Applies only to the obsolete NQO panelboards (these panelboards accepted only plug-on type breakers)

Cause:
There is a need to replace a Q1 breaker in an obsolete NQO panelboard

Resolution:
This Q1 circuit breakers are obsolete. In the obsolete NQO panelboard, the Q1 breaker can be replaced with a QO breaker and an SK5669 mounting kit.
Was this helpful?
What can we do to improve the information ?