Technical FAQs

Ask a Question

What is the part number for the removable handle lock off attachment for EDB breakers in NF panelboards?

Issue:
Need to lock off handle on E frame breakers

Product line:
Powerpact E frame

Environment:
NF panelboards

Cause:
Need to lock the handle in OFF position for maintenance or safety.

Resolution:
Use the HPAFD lock off device.
Can be used with a padlock (provided by customer) or the screw that is included in kit.
The removable padlocking device HPAFD is the only handle padlock attachment that will work with the Series 1 - EDB, EGB and EJB breakers.
It will work with 1, 2 and 3 pole breakers and will lock them in the Off position only.
Not for use on EH or EHB breakers.





CTA-ID : 1247
Was this helpful?
What can we do to improve the information ?