Technical FAQs

Ask a Question

What is the 120 volt replacement coil for a Type SA NEMA size 00 contactor or starter?

The 120 vac replacement coil for all Size 00 contactors depends on the device`s series or revision. The following outlines the part by Series number:
Series A 60hz - 31041-400-42
Series A 50hz - 31041-400-43
Series B - 9998SAC45.
For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 2157
Was this helpful?
What can we do to improve the information ?