Technical FAQs

Ask a Question

What are the 120-volt latch and unlatch coils for 8903LX lighting contactors?

The 120-volt unlatch coil is part number 9998LX44, for the latching coil there is one for the 2 to 6 pole contactor which is 9998L44 and one for the 8 to 12 pole contactor which is 9998LH44.

CTA-ID : 1845
Was this helpful?
What can we do to improve the information ?