Technical FAQs

Ask a Question

What is the stand alone withstand rating of Class 8910 Type DPA contactors?

The DPA device conforms to the UL Standard for withstandability which is as follows; devices with maximum horsepower rating of 1/2 to 50 horsepower 5,000 amps, devices with maximum horsepower rating of 51 to 75 horsepower 10,000 amps.


CTA-ID : 1642
Was this helpful?
What can we do to improve the information ?